Gauge Properties - General tab

The following table shows options in the
General
tab.
Options
Description
Back style
Select whether the object background is solid, gradient, or transparent. If you select Transparent, the object’s background is not filled in and any objects behind it show through. If you select Gradient, the object's background is filled with a linear gradient color.
Line style
Select the line style. If you select a style other than Solid, the line width must be 1 pixel.
The line properties apply to the dial outline and tick marks.
Line width
Type the number of pixels for the width of the object's line. Any line style other than solid must have a width of 1 pixel.
Sweep style
Specify whether or not to color the area behind the needle as the value changes. Select solid fill or gradient fill, if you want to use the fill color to color the portion of the gauge that has a value less than or equal to the Value control. Select Point to point the needle at the value of the Value connection.
Needle width
Type the number of pixels for the width of the gauge’s needle.
Major ticks
Select the number of major ticks. You must use at least two major ticks (one for each end of the dial).
Minor ticks
Select the number of minor ticks. This number of ticks appears between each major tick.
Font
Select the font to use for the legends. Specify whether to use legends in the Display tab.
Size
Select the font size to use for the legends.
Bold (B), Italic (I), Underline (U)
Click a letter, or letters, to specify the font style for the caption, if required.
Back color
This field displays the current background color for the object or state. Click it to select another color. If the background style is transparent, the application does not use this background color. If the background style is gradient, click it to bring up the gradient fill dialog box to configure the gradient fill. For objects with a line style other than Solid, the background color is used for the spaces between the dots or dashes.
Fill color
This field displays the current fill color for the gauge. Click it to select another color. If the sweep style is gradient, click it to bring up the gradient fill dialog box to configure the gradient fill. This color is not used if you select Point for the sweep style.
If you specify thresholds for the gauge, you can also assign a fill color to each threshold in the Display tab.
Needle color
This field displays the current needle color for the gauge. Click it to select another color.
Fore color
This field displays the current color for the object’s text or line. Click it to select another color.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal