TriggerType
Select Value if the object is to trigger the state whose State Value property corresponds to the value of the Value connection.
Select LSB if the object is to trigger the state whose State Value property corresponds to the position of the least significant bit (LSB) in the object's Value connection.
TIP:
The LSB trigger type does not work with Default data type because the LSB trigger type does not support Floating point numbers.
The following table shows how the value of the Value connection corresponds the value of the State Value property if the TriggerType property is set to LSB.
This Value connection value | triggers this State Value |
|---|---|
0 | 0 |
1 | 1 |
2 | 1 |
4 | 2 |
8 | 3 |
16 | 4 |
Provide Feedback