ImageBackColor or St_ImageBackColor

This property applies only to monochrome images. It determines the color of the background the image is drawn on.
If the ImageBackStyle property is set to Transparent, the background of the image will be transparent. To select another color, double-click the colored box to open the color palette. Click a color to select it, or click Other to create a custom color.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal