HighlightColor
The box displays the current highlight color. Double-click it to open the color palette and select another color. Click a color to select it, or click Other to select from a broader range of colors.
The object’s border, if it has one, changes to the highlight color when the operator presses the object at runtime.
Provide Feedback