HandshakeResetType
Specifies how the Enter Handshake connection resets the Enter connection to zero (0):
- Non-zero valueresets the Enter connection when the Enter Handshake connection is a non-zero value.
- Zero to non-zero transitionresets the Enter connection when the Enter Handshake connection changes from 0 to a non-zero value.
Provide Feedback