FillColor for the SweepStyle property
Specifies the fill color for the object. This color is used only if you select Fill for the SweepStyle property. Double-click it to open the color palette and select another color. Click a color to select it, or click Other to select from a broader range of colors.
If you specify thresholds for the object, you can also assign a fill color to each threshold.
Provide Feedback