BackColor or St_BackColor

Displays the background color for the object or state. Double-click it to open the color palette and select another color. Click a color to select it, or click Other to select from a broader range of colors.
If the BackStyle property is Transparent, the background color is not used. For objects with a LineStyle property other than Solid, the background color is used for the spaces between the dots or dashes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal