Options of completing creating a firmware upgrade card
The following table describes the options of completing creating a firmware upgrade card.
Option | Description |
|---|---|
Upgrade type | This shows the type of upgrade you selected: Firmware upgrade card . |
Terminal Type | This is the terminal you selected.. |
Upgrade firmware version | This shows the version of the firmware that you have selected as the upgrade for the terminal. |
Firmware card location | This is the folder you specified for the firmware upgrade files. It should be either a local disk such as F:\ , or a location on your local disk drive, such as C:\Firmware . |
ViewPoint | This shows whether FactoryTalk ViewPoint is included in the firmware upgrade. |
KEPServer drivers | If you select any KEPServer drivers, they shows here. |
Provide Feedback