Options of completing the remote terminal firmware upgrade
The following table describes the options of completing the remote terminal firmware upgrade.
Option | Description |
|---|---|
Upgrade type | This shows the type of upgrade you selected: Terminal firmware upgrade . |
Terminal Type | This is the PanelView Plus 7 or PanelView Plus 6 terminal you selected in the FactoryTalk Linx communications tree or (if you are using an Ethernet or serial connection) found with the File Transfer Utility. |
Current firmware version | This shows the firmware version presently installed on the selected terminal. If this shows Unknown , the firmware on the terminal is damaged. |
Upgrade firmware version | This shows the version of the firmware that you have selected as the upgrade for the terminal. |
ViewPoint | This shows whether FactoryTalk ViewPoint is included in the firmware upgrade. |
KEPServer drivers | If you select any KEPServer drivers, they shows here. |
Provide Feedback