Start
FactoryTalk® Remote Access

NOTE: If you have concerns regarding your privacy or wish to exercise your data rights, including access, correction, or deletion of personal information, contact the Technical Support Team. They are trained to assist with all data-related inquiries in accordance with applicable privacy regulations.
  1. To start
    FactoryTalk® Remote Access
    you must access
    FactoryTalk® Hub
    first. Before accessing
    FactoryTalk® Hub
    , you must Create your MyRockwellAutomation account.
  2. Once you have your MyRockwellAutomation account, Log in to FactoryTalk Hub.
  3. To use
    FactoryTalk® Remote Access
    , you must belong to a
    FactoryTalk® Hub
    organization. See Create an organization and a domain.
    TIP: A company is typically associated with an organization that company users can join. All of the entitlements activated for a company are allocated to the organization.
  4. Access
    FactoryTalk® Remote Access
    by clicking on the related tile.
    TIP: If you have a MyRockwellAutomation account and belong to an organization, you can start
    FactoryTalk® Remote Access
    directly by typing
    ftra.cloud.rockwellautomation.com/oauth
    in your browsing bar.
    Sign in, and if you belong to multiple organizations, select one by clicking the down arrow next to the user icon in the top right corner.
    NOTE: The inactivity timeout for
    FactoryTalk® Remote Access
    Manager is set to 30 minutes. After this period, you will be automatically logged out unless a VPN connection is established, such as through the
    Interactive Access (Web-only)
    or while a VPN connection is enabled via the
    Interactive Access (Tools)
    . In this case, you will not be logged out.
  5. (optional) To set up your language, see Language setup
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal