Studio 5000 Logix
Designer® and
FactoryTalk® Design Studio™
Integration
Studio 5000 Logix
Designer®
and
FactoryTalk® Design Studio™
Integration
FactoryTalk® Optix™
provides tag import for applications that are authored
in Studio 5000 Logix
Designer®
and
FactoryTalk® Design Studio™
. To import tags from these applications:
- InFactoryTalk® Optix™, open your project and start the Configure Communications wizard.
- Choose New Station and select RAEtherNet/IPstation.
- In Route, use either a plain IP (slot 0) or the backplane to target another slot.
- Choose either:
- Online to importStudio 5000 Logix Designer®orFactoryTalk® Design Studio™tags directly from the controller
- Offline to import aStudio 5000 Logix Designer®project (file type .ACD, .L5X, or .L5K).
- Imported tags show in Project View > CommDrivers > RA EtherNet_IPDriver > ? > Tags. Assign your tags to widgets and logic.
Provide Feedback