Quick Start with FactoryTalk® Optix™
FactoryTalk® Optix™
For quick start information, see the following resources.
- FactoryTalk Optix Resources - Explore manuals, online help, diagrams, tutorials, videos, and more.
- FactoryTalk Optix Software Platform - See the Resources tab.
- FactoryTalk Optix organization on GitHub - Contains a set of repositories that you can use as POC, training, or demonstrations.
Provide Feedback