FactoryTalk® Remote Access™
FactoryTalk® Remote Access™
The
FactoryTalk® Remote Access™
solution supports the maintenance of operations with
remote access via VPN. Also, in situations where operational plants are remote, the solution
lets you investigate and resolve issues before planning travel to the site.With
FactoryTalk® Remote Access™
Manager software, you can manage machines from a
centralized web-based interface to perform, configure, and operate the VPN tunnel for remote
access. You can apply two-factor authentication to validate the user identities. In addition,
the Transport Layer Security (or TLS) encryption protocol ensures confidentiality, integrity,
and authenticity of the data exchange session. Logs and audit trails are available for
tracking remote access operations and established connections.The
Stratix®
4300 remote access router adds hardware to the
solution. The router lets machine builders and OEMs operate on remote systems and its
subnetworks. The routers are offered in two and five 10/100/1000 Mbps Gigabit Ethernet copper
port variants.FactoryTalk® Remote Access™
Architecture
Provide Feedback