Application Code Libraries/Trusted Content
Rockwell Automation®
has built libraries of standard application content to help
you easily integrate automation products into systems. This application content helps
engineers create automation projects from standardized, lifecycle-managed, application-focused
libraries in an efficient way. Reduce design cost, build projects faster, and drive consistent results with the
Rockwell Automation®
Library of Process Objects ( PlantPAx®
Libraries), Device Object Libraries, and Machine Builder Libraries.The following libraries and version of
FactoryTalk® Optix™
are compatible:Library | FactoryTalk® Optix™ 1.5 Compatible Version | FactoryTalk® Optix™ 1.4 Compatible Version |
|---|---|---|
Power Device | 3.06 | 3.05 |
Safety Device
| 1.06 | 1.05 |
Network Device
| 12.05 | 12.04 |
Condition Monitoring Device
| 1.03 | 1.02 |
Hardy Device
| 1.01 | 1.00 |
IO Device
| 5.05 | — |
IO-Link Device
| 3.03 | — |
Mettler Toledo Device
| 1.01 | — |
Plex APM | 1.01 | 1.00 |
Plex QMS
| 1.01 | 1.00 |
Fiix®
| 1.01 | 1.00 |
You can download the libraries at the Product Compatibility and Download Center (PCDC). The
PCDC is available at rok.auto/pcdc.
1
For more information, see
Power Device Library Reference Manual, publication DEVICE-RM100
2
For more information, see
FactoryTalk® Optix™
Plex APM Library
Object Reference Manual, publication INFO-RM005Provide Feedback