Configure temperature controls

Create Label, Textbox, and Linear gauge objects to visualize and control the temperature variable.
  1. In
    Project view
    , double-click
    Page1 (type)
    .
    Page1 (type) opens in the editor.
  2. Right-click
    Page1 (type)
    and select
    New
    Base controls
    Label
    .
  3. In
    Properties
    , set
    Text
    to
    Temperature:
    .
  4. In
    Project view
    , right-click
    Page1 (type)
    and select
    New
    Base controls
    Text box
    .
  5. In
    Properties
    , create a dynamic link between
    Text
    and the
    Temperature
    variable.
    TIP: You can create the dynamic link by dropping the
    Temperature
    variable from
    Project view
    into the
    Text
    property value of the
    Text box
    in
    Properties
    .
    For more information about dynamic links, see Create dynamic links.
  6. In
    Project view
    , right-click
    Page1 (type)
    and select
    New
    Base controls
    Linear gauge
    .
  7. In
    Properties
    , create a dynamic link between
    Value
    and the
    Temperature
    variable.
    For more information about dynamic links, see Create dynamic links.
  8. In the editor, arrange the objects according to your preferences.
Temperature controls in the top-right corner
The user interface displays a temperature slider control, a spin box, a toggle
            switch, and an LED in the center on a grid background.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal