Configure a recipe

Create a recipe schema that uses the Ingredient01, Ingredient02, and Ingredient03 variables.
For more information, see Configure a recipe schema.
  1. From the toolbar, select
    Open dashboard page icon
    Open dashboard page
    .
  2. In the editor, select
    Configure a recipe
    .
  3. Select
    New recipe
    .
  4. In
    Name
    , enter a name for the recipe schema, and select
    Next
    .
  5. In
    Target node
    , select the project node that contains the variables to use as ingredients and select
    Next
    .
    The target node can be the
    Model
    folder, an object inside the
    Model
    folder, or a node with variables from controllers.
    TIP: To define variables from several nodes as ingredients, create a dedicated object in the
    Model
    folder and add variables inside it. Then, create a dynamic link between the variables and the ingredients. Selecting this object as the target node makes ingredient selection easier.
  6. Select
    New database
    .
  7. In
    Name
    , enter
    RecipeDB
    and select
    Next
    .
  8. Select the variables to use as ingredients (for example,
    Ingredient01
    ,
    Ingredient02
    , and
    Ingredient03
    ), and select
    Next
    .
  9. Review the recipe summary, and select
    Exit
    .
In
Project view
,
RecipeSchema1
appears under
Recipes
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal