Add graphic objects

Add a Switch, Spin box, and LED objects to Page1 of your application.
  1. In
    Project view
    , double-click
    Page1 (type)
    .
    Blank Page1 displays in the editor in a separate tab.
  2. Right-click
    Page1 (type)
    and select
    New
    Base controls
    Switch
    .
  3. Right-click
    Page1 (type)
    and select
    New
    Base controls
    Spin box
    .
  4. Right-click
    Page1 (type)
    and select
    New
    Base controls
    LED
    .
  5. In the editor, arrange the objects according to your preferences.
Arranged graphical objects
The workspace displays a grid background with a spin box and a toggle switch in the
            upper left, and an LED in the center.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal