TrendPen.RemoveYAxis()
Removes the Y-axis from the trend pen.
public static void RemoveYAxis(this TrendPen pen)
Arguments
- pen
- The trend pen to get or add the Y-axis to.
Exceptions
- ArgumentNullException
- Thrown when no validpenis provided.
Example
The following example shows how to remove the Y-axis from a trend pen:
// Remove the Y-axis from an existing pen var pen = Project.Current.FindObject("MyTrendPen") as TrendPen; pen.RemoveYAxis();
Provide Feedback