Configure a recipes editor
You add a recipes editor widget by selecting it from the template libraries and editing its properties.
Prerequisites
- To configure a recipes editor
- From the toolbar, select.Template Libraries
- InTemplate Libraries:
- SelectWidgets.
- DragRecipes Editorto theUIfolder inProject view.
- SelectClose.
- InProject view, create an instance ofRecipeEditor (type).
- InProperties, in theRecipeSchemaAliasproperty, select aRecipe Schemaobject that you want to use.
- (optional) InProperties, configure theAppearance,Size and layout, andEventoptions.
Provide Feedback