UX design for UI objects

Designing user interfaces that are consistent, intuitive, responsive, and accessible is key to delivering a seamless user experience.

Consistency and intuitiveness

Design intuitive and consistent UI behavior to enhance usability and ensure predictable user interactions.
  • Keep UI behavior predictable. For example, buttons should always look clickable.
  • Ensure frequently used UI elements are easily accessible.

Responsiveness

Design responsive UI elements that adapt seamlessly to different screen sizes and devices for a consistent user experience.
TIP: See Create a responsive user interface for further information on this topic.
  • Ensure UI objects adapt to different screen sizes.
  • Test the UI on various devices to verify consistency.

Accessibility

Design UI elements with sufficient contrast and full keyboard and screen reader support to ensure accessibility for all users.
TIP: See Style sheets for further information on this subject.
  • Use sufficient contrast for readability.
  • Ensure interactive UI objects are keyboard and screen reader accessible.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal