Add a client device
Configure a client device to allow the deployment of
FactoryTalk Optix Applications
over the network.- From the main toolbar, next to, select the client dropdown menu.Run
- (optional) InClient device settings, to display only the active remote client devices, toggleActive remote devices.TIP: Refresh remote client devices by selectingRefresh.
- Select either:
- A folder and select.

- AFactoryTalk® Remote Access™device and selectto add a device accessible from the selected
FactoryTalk Remote Accessdevice network.
- (optional) InName, edit the name of the target device.IMPORTANT: Only alphanumeric characters are allowed in the name.
- InIP Address, enter the IP address of the target device.
- InUsername, enter the name of the user to log on to the target device.
- Windows®username
- A system username:
- DOMAIN\, for domain users.username
- , for local users on domain-joined devices..username
- , for local users on devices that do not belong to a domain.username
- Linux username
- An administrator username.
IMPORTANT: A password must be configured for the user on the target device. - (optional) SelectEncrypt project on deviceto encrypt the deployed project on the target device.For more information, see Project encryption.
- (optional) SelectDownload source project on deviceto download the source project on the target device.TIP: Downloading the source project on the target device enables you to upload the source project from the target device to the development computer later on. For more information, see Open a project.
- (optional, only forWindowsclient devices) InDestination Path, enter the path on the target device to deploy the application.TIP: The default deployment destination path is%localappdata%. Defining a custom path is useful when theC:\partition of the client device is write-protected.
- ChooseSelectto select the target client device.
Provide Feedback