SQL queries
Use the ANSI SQL-92 standard for querying ODBC databases and embedded databases.
Statements
FactoryTalk Optix Studio
supports these statements in SQL queries:
- SELECT
- DELETETIP: Run aDELETEquery to delete a record. You can perform all other operations by using the OPC UA methods exposed by the same objects. For more information on the SQL statements and clauses, see the SQL standard.
- UPDATE
FactoryTalk Optix Studio
partially supports these statements in SQL queries:
- CREATE
- DROP
Literal values
Literal value type | Example | Notes |
|---|---|---|
Integral | 1520 | Do not use any thousands separators. Use the Int32 type. |
Real | 15.025 | Use . as the decimal separator.Use the Double type. |
Real scientific | 2.7000001072883606E-1 | |
Boolean |
| Use lowercase for Boolean values. |
String | 'string value' | Use single quotes to delimit text. Insert a single quote ( ' ) in a text string by escaping the single quote with another single quote. For example, to write 'string' , use two single quotes ''string'' in the strings. |
Date and time | "2004-05-23T14:25:10.487" | Use the ISO8601 format delimited by double quotes. The date and time notation is non-standard ANSI SQL used to avoid the DATE , TIME , and TIMESTAMP keywords without ambiguity. |
Regular identifier |
| Do not use spaces. Start with an uppercase or a lowercase letter. You can use numeric digits, letters, and the underscore character _ . |
Delimited identifier |
| Use double quotes ( " ) as the delimiter.In the identifier, use any character except for the " character.Any spaces at the end of the identifier are ignored. |
Aliases
You can use aliases in the identifiers, derived column subqueries, and tables.
The following are examples of queries with aliases:
SELECT Timestamp AS T FROM Table1 WHERE ...
SELECT * FROM Table1 AS T WHERE ...
SELECT * FROM (SELECT * FROM Table1) AS SubQuery WHERE ...
CREATE TABLE Table1 AS SELECT Timestamp, Column1 FROM Table2
Operators
Operator | Example |
|---|---|
IN |
|
BETWEEN |
|
LIKE |
|
EXISTS |
|
IS |
|
NOT |
The NOT operator applies to all other operators. |
Window functions
Function | Example |
|---|---|
ROW_NUMBER |
|
RANK |
|
DENSE_RANK |
|
AVG |
|
SUM , MIN , MAX |
|
COUNT |
|
Provide Feedback