- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Integrate the interface with the NetLogics
Integrate the NetLogics with the application interface.
- InProject view, expand .
- Configure the Insert Random Data button:
- InProject view, selectInsertButton.
- InEvents, next toMouseClick event, selectand select .
- Configure the Display Query in Label button:
- InProject view, selectRunQueryButton.
- InEvents, next toMouseClick event, selectand select .
Provide Feedback