- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Develop a files counter
This C# solution calculates the number of files in the project folder.
Prerequisites
- To develop the project
- Create the application interface and integrate it with the NetLogic.
In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select 
Provide Feedback