Access to FactoryTalk Linx extended tag properties
FactoryTalk Linx Gateway supports access to FactoryTalk Linx extended tag properties via the
OPC UA, MQTT, OPC DA, RTD, and DDE interfaces.
- .@Timestamp
- .@Quality
- .@Name
- .@Scope
These samples assume that you have a tag named "Tag1". To view the tag's extended properties in the client, use the following samples if the namespace mode is Folders with scalar data or Tag list and structures/array access:
- [Shortcut]Tag1.@Timestamp
- [Shortcut]Tag1.@Quality
- [Shortcut]Tag1.@Name
- [Shortcut]Tag1.@ScopeTIP: If you want to view the FactoryTalk Linx extended tag properties in a program named "Program1", the sample is as follows:
- [Shortcut]Program:Program1.Tag1.@Timestamp
If the namespace mode is
Custom namespace
, map to a specific tag. For more information, see Extended tag properties.Provide Feedback