FactoryTalk Linx Data Bridge performance reference
Starting from
FactoryTalk Linx Data Bridge
version 6.20.00, the maximum number of controller tags that can be bridged via FactoryTalk Linx Data Bridge
reaches up to 200,000. There are many factors such as the computers' hardware configuration, network loading, and controller communications bandwidth could impact or prevent a system from achieving this high number of tag pairs. Rockwell Automation
tests the following scenarios with the test results as a reference.
TIP:
The following data were retrieved from a testing environment. The actual result may be different because of the changes to product firmware, software versions, system or controller network loading. The data was based on
FactoryTalk Linx Data Bridge
version 6.20.00.FactoryTalk Linx Data Bridge
reading from a single controller and writing to a different controller using the single Ethernet module:- FactoryTalk Linxdata server andFactoryTalk Linx Data Bridgeserver are installed on the same machine.
- Hardware information:Computer
- Operating system: Windows 10 Professional edition
- Processor:Intel® Xeon®W-2014 CPU @3.2 GHz
- Memory: 8 GB
Compute module- Operating system: Windows 10 Enterprise 2016 Long-Term Servicing Branch
- Processor: Intel (R) Atom (TM) CPU E3826 @ 1.46 GHz
- Memory: 4 GB
CompactLogix 5480- Operating system: Windows 10 Enterprise 2016 Long-Term Servicing Branch
- Processor:Rockwell Automation64 bit @2.39 GHz
- Memory: 6 GB
- Test results:

FactoryTalk Linx Data Bridge
reading from multiple controllers and writing to a different controller using multiple Ethernet modules:- FactoryTalk Linxdata server andFactoryTalk Linx Data Bridgeserver are installed on the same computer.
- Hardware information:Computer
- Operating system: Windows 10 Professional edition
- Processor: Intel (R) Xeon (R) W-2014 CPU @3.2 GHz
- Memory: 8 GB
Controller- 1756-L85 ControlLogix Controller
- 1756-EN2T ControlLogix Controller
- Test results:The number of data pairs is less than 100 and the tags actual update rate in the controller is 100 msData PairDB Memory (MB)Data Bridge.exe CPU (%)Destination Tag Actual Update Rate (s)2022.910.164023.910.166024.510.168025.210.1610025.610.16The number of data pairs is less than 1,000 and the tags actual update rate in the controller is 250 msData PairDB Memory (MB)Data Bridge.exe CPU (%)Destination Tag Actual Update Rate (s)20027.110.2940031.820.360037.120.380041.120.311,00043.720.32The number of data pairs is less than 10,000 and the tags actual update rate in the controller is 500 msData PairDB Memory (MB)Data Bridge.exe CPU (%)Destination Tag Actual Update Rate toFactoryTalk Linx(s)Destination Tag Actual Update Rate toFactoryTalk LinxOPCUA Connector (s)04.30002,00061.920.61.14,00098.53126,000119.831.33.18,000149.941.74.310,000178.252.15.6The number of data pairs is less than 100,000 and the tags actual update rate in the controller is 1,000 msData PairDB Memory (MB)Data Bridge.exe CPU (%)Destination Tag Actual Update Rate toFactoryTalk Linx(s)Destination Tag Actual Update Rate toFactoryTalk LinxOPCUA Connector (s)04.300010,000186.5742.15.320,000313.963.61030,000440.783.61040,000568.2113.61050,000703.8133.610.660,000833.9174.211.870,000974.2195.313.780,0001099.820715.690,0001229.4221020100,0001361.12318.530.3
Provide Feedback