Tag List
The Tag List displays details of the current tags and other data applicable to the selected tags. In the Tag List, each row represents a tag, and multiple tags are possible. A maximum of 16 tags can be added to the table and displayed on the canvas.
The following table describes the data provided for each tag.
Column | Description |
|---|---|
Style | Displays the color of the tag line. To customize the color for each tag, select
the down arrow next to the color text. |
Visible | Indicates whether the tag is visible on the trend. Select to hide a selected tag without removing it from the Tag List. The tag is also
hidden from the trend. |
Name | Displays the fully qualified name of the tag. This field cannot be changed. |
Description | Displays the descriptions of the raw tag recorded in Asset Framework or Data Archive. This field cannot be changed. |
Min Value | Displays the minimum value of the raw acquired value of the tag. This field cannot be changed. |
Max Value | Displays the maximum value of the raw acquired value of the tag. This field cannot be changed. |
Average Value | Displays the average value of the raw acquired value of the tag. This field cannot be changed. |
Action | Deletes a tag from the Tag List, which also removes it from the trend and clears its checkbox in the left pane. |
You can customize the Tag List table.
- To adjust the column width, drag the header to your preferred size.
- To rearrange the headers, simply drag them to your desired position, release the mouse, and the columns will be moved.
- To sort the tag by Style, Visible, Name, Description, Min Value, Max Value, and Average Value, click the up arrow next to these headers.
Provide Feedback
to hide a selected tag without removing it from the Tag List. The tag is also
hidden from the trend.