Add a FactoryTalk Historian SE server to a FactoryTalk Directory
Once the
FactoryTalk Historian SE
server is installed and running, add it to the FactoryTalk® Directory
.To add the
FactoryTalk Historian SE
server to the FactoryTalk Directory
- In theExplorertree, expandSystem>Connections.
- Right-clickHistorical Dataand selectNew Historian Server Connection.
- In theNew Historian Server Connectiondialog, enter theFactoryTalk Historian SEserver name or select from theServer or collective namelist.If the desiredFactoryTalk Historian SEserver is not on theServer or collective namelist, see Update the known servers table.TIP:
- A collective consists of twoFactoryTalk Historian SEservers that have the same configuration database. To create a collective, you must use the Collective Manager.
- For a Historian server collective, enter the primary server name of the collective or select the collective name from theServer or collective namelist. If the collective name is not on the list, make sure that it has been added to the Connection Manager. Then, follow the steps in the Update the known servers table.
- SelectTest server connections.
- If the connection is successful, the "Server found" message appears.
- If the connection is not successful, the "No server found" message appears. In such a case, check the status of your server in the Connection Manager.
- Do one of the following actions as needed:
- To add aFactoryTalk Historian SEserver to aFactoryTalk Directory, selectCreate.
- To add aFactoryTalk Historian SEserver to aFactoryTalk Directoryand modify theFactoryTalk Historian SEserver properties, selectCreate and configure.
The new server connection with the default Live Data interface instanceFTLD1appears under theHistorical Data>Production Historianfolder.
Provide Feedback