Exception filtering

The exception reporting information determines when to send data to the snapshot subsystem.
The Exception Filtering group contains the following point attributes:
  • Exception Min
    This value specifies the minimum time span between the exceptions.
    The default value is 0 seconds.
  • Exception Max
    This value specifies the maximum time span between the exceptions.
    The default value is 10 minutes.
  • Exception Deviation
    This value specifies how much a point value must change before a new value is reported.
    The default value is 0.25 engineering units.
The following are value ranges that you can use to specify parameter values:
  • The range of Exception Min Day and Exception Max Day is between 0 and 100.
  • The range of Exception Min Hr and Exception Max Hr is between 0 and 15.
  • The range of Exception Min Min and Exception Max Min is between 0 and 59.
  • The range of Exception Min Sec and Exception Max Sec is between 0 and 59.
  • The Exception Deviation range is between 0 and 100.
    TIP:
    For details on the exception filtering configuration, see Exception filtering.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal