Configure Resource Types
The user can edit, add, and delete the Resource Types for various resources.
Add Resource Configuration
Perform the following steps to add a new resource configuration:
- Under theResource/Utility Typestab, clickAdd.
- In theAdd Resource Configurationdialog box, set these parameters:
- Resource/Utility Type: Select a resource/utility from the dropdown list.
- Consumption Unit: Select a unit from the dropdown list.
- Consumption Decimal Place: Select a decimal place from the dropdown list.
- Demand Unit: Select a unit from the dropdown list.
- Demand Decimal Place: Select a decimal place from the dropdown list.NOTE:Consumption Unit,Consumption Decimal Place,Demand Unit, andDemand Decimal Placeare enabled on selecting a specific resource type.
- ClickAdd.Add Resource Configuration
The "Added successfully” message is displayed. User can add multiple resource/utility types.
Resource/Utility Types
Resource/ Utility | Icon | Type |
|---|---|---|
Electricity | Energy | |
Natural Gas | Energy | |
Biogas | Energy | |
Propane | Energy | |
Hydrogen | Energy | |
Diesel Oil | Energy | |
Fuel Oil | Energy | |
Gasoline | Energy | |
Crude Oil | Energy | |
Coal | Energy | |
Tallow | Energy | |
Water | Non-Energy | |
City Water | Non-Energy | |
Waste Water | Non-Energy | |
Ground Water | Non-Energy | |
Compressed Air | Utility (Derived Energy) | |
Chilled Water | Utility (Derived Energy) | |
Hot Water | Utility (Derived Energy) | |
Hot Hot Water | Utility (Derived Energy) | |
Steam, Saturated | Utility (Derived Energy) | |
Steam, Superheated | Utility (Derived Energy) | |
Virtual Meter Icons | The Virtual Meter icon is identified by a dotted border around the corresponding
resource or utility type icon. Example: | |
Edit Resources Configuration
Perform the following steps to edit the resource type details:
- In any site dashboard, under theConfigurationsection, theResource/Utility Typestab is displayed by default.Resource Types
TheResource/Utility Typetab displays all the available resource types. - On the required resource type, click the [
] icon. - In theEdit Resource Configurationdialog box, edit the fields and clickSave.Edit Resource Configuration
The "Updated successfully” message is displayed.
Delete Resource Configuration
Perform the following steps to delete the resource configuration:
- Under theResource/Utility Typestab, on the required resource/utility type, click the [
] icon. - In theDelete Resource Type Configurationdialog box, clickDelete.
The “Delete Resource Type Configuration
Deleted successfully” message is displayed.
Provide Feedback