Edit a model
Edit models at any time. Redeploy the applications to see the changes.
TIP:
FactoryTalk Smart Object
models are not editable.To edit a model
- Perform one of these actions:
- SelectData Flow>Models.
- SelectData Flowand then underOrganize, selectConfigure.
- SelectEdit
next to a model. - Edit the model.
- SelectSave.
- Review and redeploy any dependent applications.
Provide Feedback