Delete a model
Delete a model to remove it from the list of available models. It is only possible to delete a model that an application has not configured for use.
To delete a model
- Perform one of these actions:
- SelectData Flow>Models.
- SelectData Flowand then underOrganize, selectConfigure.
- (optional) Filter the list of models.
- Select the models to delete.
- SelectDelete
. - SelectSave.
Provide Feedback