Bind tags to a model
Tags are elements of information from your data source. After adding a model and staging tags, associate tags to elements (nodes and properties) in the model.
TIP:
Tags are automatically bound in
FactoryTalk Smart Object
models.To bind a tag to a model
- Perform one of the actions:
- SelectData Flow>Models.
- SelectData Flowand then underOrganize, selectConfigure.
- SelectEdit
next to a model. - (optional) Filter the list of tags.
- Perform one of these actions:
- To select and bind multiple tags, underTags, select the tags to associate to the node or property and then selectBind. The tags appear underneath the top-level node.
- Select a tag, select a node or a property and then selectBind.
- Drag and then drop a tag on a node or a property.
- SelectSave.TIP:To unbind tags from a model, select the tags in the model and then selectUnbind.
Provide Feedback