Gateway Status
The
Gateway Status
displays data about the computer running FactoryTalk Edge Gateway
and licensing information:Data | Description |
|---|---|
Total Memory | The total amount of RAM installed in the computer running the gateway. |
Free Memory | The amount of RAM currently available in the computer running the gateway. |
CPU | The percentage of the central processing unit (CPU) that FactoryTalk Edge Gateway currently uses. |
Licensed Tags | The total number of licensed tags that all deployed applications use. If multiple applications use a tag, the tag is only counted once. |
Maximum Licensed Tags | The maximum number of licensed tags available (100, 500, 2500, or 10000) based on the tag activation in use. |
License Status | Displays the current license status:
|
Provide Feedback