Data Out
Data Out
displays information about applications flowing out of the gateway:Status icon | Name | Licensed tags |
|---|---|---|
![]() | The name of the stopped application. | Stopping an application frees the licensed tags so that they are available for use by other applications. |
![]() | The name of the paused application. | The quantity of licensed tags that the paused application uses. |
![]() | The name of the running application. | The quantity of licensed tags that the running application uses. |
Provide Feedback