Data In
Data In
displays information about data sources flowing into the gateway:Column | Description |
|---|---|
Name | The name of the configured data source. |
Driver | The name of the driver defined for the data source. The driver displays one of these statuses:
|
Collection Path | The collection path defined for the data source. The collection path displays one of these statuses:
|
Provide Feedback
The driver is stopped.
The driver is paused.
The driver is running.