Start, stop, and pause a driver
Start, stop, and pause gateway drivers as needed. Pause a driver to stop incoming or outgoing data. The paused driver still exists on the gateway. Stop a driver to remove it from the gateway. The stopped driver is still available in the gateway configuration. You cannot stop a driver used by a running application.
To start, stop, and pause a driver
- SelectData Flow>Data Sources.
- FromDefine Drivers:
- SelectRun
to start the driver. - SelectPause
to pause the driver. - SelectStop
to stop the driver.
Provide Feedback