Edit a driver
Edit an existing driver to modify the settings. Go
Online
to edit a driver.
TIP:
You cannot edit a driver in use by a running or paused application. Stop the dependent application to edit the driver.
To edit a driver
- SelectData Flow>Data Sources.
- (optional) FromDefine Drivers, filter the list of drivers.
- SelectEdit
for the required driver. - Modify the driver settings, and then selectSave.
Provide Feedback