ThingWorx template and shape mapping rules
ThingWorx
template and shape mapping rulesFactoryTalk Edge Gateway
node properties map to properties inherited from a ThingWorx
template or shape. If the node uses a ThingWorx
template or shape but contains properties that are not in the ThingWorx
template or shape, FactoryTalk Edge Gateway
creates the corresponding properties on the target Thing.To achieve correct property mapping across properties, set these properties in
ThingWorx
Composer. - Base Thing Template- SelectRemote Thing.TheBase Thing Templatesetting can be anotherThingWorxtemplate or shape if the underlyingThingWorxtemplate or shape is based on a remote Thing.
- Name- Name of the property. The name must match theFactoryTalk Edge Gatewayproperty name exactly.
- Base Type-Select the base type (data type). The base type must match the data type of theFactoryTalk Edge Gatewayproperty.FactoryTalk Edge Gatewaydata typeThingWorxbase typeSTRINGSTRINGDINTIntegerLINTLongREALNumber
- Binding- SelectRemotely Bound.
Provide Feedback