Add an application
Add applications to
FactoryTalk Edge Gateway
to send data to the required server or IoT device. After adding an application, configure the models or tags to bind them to the application.
TIP:
The maximum number of applications that are permitted for each gateway instance are:
- SQL Serverand Azure IoT Hub: Five applications
To add an application
- In the top-right corner, selectOnlineto go online with the gateway.FactoryTalk Edge Gatewaydisplays a green banner:Gateway Connection: Online.
- SelectData Flow>Applications.
- To add the first application, selectAdd Application.
- To add a subsequent application, selectAdd
.
- FromSelect Application, select an application
- SelectNext.
- Enter the application name.
- For Azure IoT Hub, MSSQL, and ThingWorx applications, configure the applicationsettings and Store and Forward settings.
- SelectSaveto add the application.
Provide Feedback