Safety Assessment
An independent, third-party review of the safety system can be required before the system
is approved for operation. An independent, third-party validation can also be required
for IEC 61508 SIL 2 or SIL 3 levels. For more information about safety assessments, see
the Machinery Safebook 5 - Safety related control systems for machinery, publication
number SAFEBK-RM002.
Provide Feedback