Known anomalies inherited from previous releases

The list identifies
FactoryTalk Design Studio
version 2.06.00 known anomalies from previous releases that are still known in this release. Use the identification information provided in the anomaly heading to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
Known anomalies from
FactoryTalk Design Studio
version 1.08.00
  • Exporting a
    FactoryTalk Design Studio
    project to the
    Logix Designer
    application fails to download due to the parameters External Access being incorrect. First identified in version 1.08.00.
    [Jira 3520069]
    To work around this issue, change the parameter's External Access setting to Read-Only.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal