Corrected anomalies in this release

The list identifies the anomalies corrected in
FactoryTalk Design Studio
version 2.06.00. Use the identification information provided in the anomaly heading to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
  • Unable to pull subsequent remote changes for projects that were renamed when copied from another organization
    For projects containing safety content that were renamed when copied from another organization, subsequent changes made by another user cannot be pulled from the remote. First identified in version 2.05.00.
    [Jira 5596502]
  • Unable to delete safety signatures at deployment
    When the controller is in Run mode, safety signatures cannot be deleted at deployment. First identified in version 2.05.00.
    [Jira 5668254]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal