Edit a tag
Edit a tag for a program, routine, controller scope, or device tag to change the tag or any
of the tag parameters. All changes to a tag are propagated throughout the scope of the
tag.
- On the explorer, go to the
Systemview, the
Executionview, or the
Libraryview. - Right-click a controller, a program, a routine, or an add-on instruction, and then selectTags and parameters.TIP: You can also select
View tags and parameters: (item name). - In the Tag Editor, change any cell in the row of a tag to change:
- Name. Type the name of the tag or program parameter.
- Data Type. Type the name of the data type until the data type appears or browse to openSelect Data Type, select the data type from the list, and then selectApply.
- Value. Enter the value of the tag.
- (optional)Description. Enter a description of the tag to indicate the purpose of the tag or the latest change to the tag.
- Scope. The scope of the tag. The scope is read-only and determined by the item inSystemfrom which you openTags and parameters.
- (optional)Style. For a BOOL, SINT, INT, DINT, or REAL tag, select a display style to define how the tag value appears. Styles include BINARY, DECIMAL, HEX, OCTAL, ASCII, EXPONENTIAL, and FLOAT.
- Usage. Select a usage type -- LOCAL, INPUT, OUTPUT, INOUT, or PUBLIC.TIP: Select a tag in the Tag Editor to edit the parameters of the tag inProperties.
- Connections. Displays the configured connection or, if more than one, the number of configured connections. Refer to View program parameter connections.
Provide Feedback