Tag references tab
The tag references tab displays the path to the tag and the number of references to the tag that exist in the routines of the project. Cross-references search for all instances of base and alias tags.
For each reference, the tag references tab displays the:
- Name/Type. The name of the instruction in the routine where the tag exists.
- Tag. The name of either the base tag or alias tag.
- Routine. The name of the routine in which the tag exists.
- Location. Where the reference can be found in the routine.
Open the tag from either the Ladder Diagram or Tag Editor.
- From the Ladder Diagram, right-click the tag and selectFind all references.
- From the Tag Editor, right-click the first cell of the tag row and selectFind all references
For more information about cross-references, see Search for cross-references.
Provide Feedback