Delete a tag

Delete a tag from the Tag Editor. Deleting a tag removes the tag throughout the project.
  1. On the explorer, go to the System Icon
    System
    view, the Execution Icon
    Execution
    view, or the Library Icon
    Library
    view.
  2. Right-click a controller, a program, a routine, or an add-on instruction, and then select
    Tags and parameters
    .
    TIP: You can also select Tags icon
    View tags and parameters: (item name)
    .
  3. In the Tag Editor, select the row header cell of the tag to delete.
  4. Press
    Delete
    or right-click the selected row and select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal