Select the controller mode

After you deploy a project to a controller, you can go online with it. Once online, use the
Online
pane to select the controller mode.
Keep these considerations in mind when selecting the controller mode:
  • When you deploy a project to multiple physical controllers, all controllers remain in Program mode. The controllers remain in Program mode until you go online with each controller and set the mode to Run.
  • You can be online with only one controller at a time. If you are currently online with a controller and choose to go online with a different controller, you automatically go offline with the current controller and all monitoring tabs are closed.
  • On the
    Online
    pane, select a mode:
    • Program
      . The controller halts execution of tasks, programs and routines. It continues to read and write I/O, but output values do not change because the program scans are not running.
    • Run
      . The controller schedules tasks, scans programs and routines, and reads and writes I/O.
    • Remote Program
      . Remote Program mode functions like Program mode except you can change the controller mode.
    • Remote Run
      . Remote Run mode is identical to Run mode except you can edit the project online and change the controller mode.
    TIP: You might need permission to select the controller mode. See User roles and access for more information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal