Deployment validation

Pre-deployment

When deploying a controller application, if there is a warning or error in any controller to which you are deploying,
Pre-deployment issues
opens with a list of controllers, statuses, and issues. Controller statuses include:
  • Warnings
    . Recoverable issues that require user approval to automatically resolve the issue during deployment. For example, you could approve automatic clearing a major fault present in the controller or changing the port mode of the controller.
  • Errors
    . Non-recoverable issues that cannot be resolved. The controller application will not be deployed to the target device.
Review the warnings and errors for each controller application to be deployed:
  • If only warnings appear, select all the issues to acknowledge that they will be resolved during deployment and then select
    Next
    .
    • If it is undesirable to deploy to the target device due to the warnings, you can select
      Next
      without selecting all of the displayed issues. If you do not select all issues, the controller application will not deploy to the target device.
  • If any error conditions appear, the controller application will not deploy to the target device. Select
    Next
    .
After all controller application pages are reviewed, a summary appears to indicate which controller applications will and will not deploy to their respective target devices.

Deployment

If there are errors during deployment, check the View messages and status with the Output pane for messages. Check the Online pane for controller status and messages.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal