Create a rules file
Prompt the AI Agent to create a rules file based on the
project or the uploaded design assets. When creating a rules file from the project, the
AI Agent populates each section using known project information. This information can
include tag naming patterns, controllers, devices, programs, routines, and
Add-On-Instructions.
- In theAI Agentexplorer, selectAI Agent session.
- InAI Agent Session, do one of the following:
- To create a rules file from the project, promptCreate a rules file for this project.in Plan or Build mode.TIP: You can also describe the standards to enforce and ask the AI Agent to include them in the rules file. For example:Always use Ladder,Every tag starts with the area code, orNever use OTL/OTU.
- To create a rules file from the uploaded design assets, prompt the AI Agent to use one or more uploaded assets. For example,Create a rules file using the standards from the control narrative PDF and the I/O list.
- Review the generatedrules.mdfile and ask the AI Agent to revise it if needed.
Provide Feedback