Data type members

There are two kinds of data type members:
  • Bit member—a member in which only a single bit of information is accessed.
  • Nonbit member—a member that is defined as another data type, such as SINT, INT, DINT, and COUNTER.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal